cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 and SSD1963 noise problem

respected
Associate II
Posted on December 09, 2013 at 15:02

I have 7'' TFT  with SSD1963 chip. I  noticed that there is a picture on the screen, but there is a big problem. As soon as I touched the screen body anywhere , the screen was dark. In addition,  when I replaced software , the screen started working , but it started being dark again. 

In fact, I have a power supply. It has 1.2V 3.3V and 5.0V at 3A. My controller is STM32F4. 

I used FSMC

https://www.youtube.com/watch?v=8GR6RkV7kRo

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on December 09, 2013 at 15:29

Looks to reset your system, rather than ''noise'', consider if you have effective grounding and supply connections.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
respected
Associate II
Posted on December 09, 2013 at 16:21

I used STM32F4 board and original STM32 ext BB board. Power supply hasn't noise. Because I saw on the oscilloscope. When I disconnected power supply and board, Noise is not there. If I connect board and power, I have seen noise signal on the scope. 

Maybe caused by FSMC.