cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f2xx USB potential bug

dcurran2
Associate II
Posted on June 21, 2013 at 13:59

search for CBW_CB_LENGTH

typedef union _USBH_CBW_Block

{

  struct __CBW

  {

    uint32_t CBWSignature;

    uint32_t CBWTag;

    uint32_t CBWTransferLength;

    uint8_t CBWFlags;

    uint8_t CBWLUN;

    uint8_t CBWLength;

    uint8_t CBWCB[16];

}field;

  uint8_t CBWArray[31];

}HostCBWPkt_TypeDef;

both are used in the code as follows

      for(index = CBW_CB_LENGTH; index != 0; index--)

      {

        USBH_MSC_CBWData.field.CBWCB[index] = 0x00;

      }   

lint produces the following

Warning 661: Possible access of out-of-bounds pointer (1 beyond end of data) by operator '[' [Reference: file ..\..\STM32_USB_HOST_Library\Class\MSC\src\usbh_msc_scsi.c: lines 307, 309]

anyone know why the code has been written this way

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
dcurran2
Associate II
Posted on June 21, 2013 at 14:26

anyone know why this has been done as follows  

    for(index = USBH_MSC_CSW_LENGTH; index != 0 ; index--)

        {

          USBH_MSC_CSWData.CSWArray[index] = 0;

        }

rather than 

 for(index = 0; index < USBH_MSC_CSW_LENGTH; index++)

alexandr
Associate II
Posted on June 21, 2013 at 17:04

Downstreaming cycle usially works faster then upstreaming.

dthedens23
Associate II
Posted on June 21, 2013 at 17:38

or use memset   with argument of sizeof() because the compiler often does not lie about sizeof()

billr1
Associate II
Posted on June 23, 2013 at 21:36

Regardless of why it was written the way it was, it certainly looks like a bug to me. It should be:

  for(index = CBW_CB_LENGTH-1; index !=0; index--)

As originally written it will overwrite the next byte in memory which may or may not cause problems, depending on what is sitting there.

 

dcurran2
Associate II
Posted on June 24, 2013 at 17:47

same could apply to

USBH_MSC_CSW_LENGTH

I only found and bothered about these as I use lint on all my projects and was doing the preparation before a peer review

It doesnt seem to affect the performance of my USB functionality but the code maybe doesnt do what the author intended