cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F20x has two OTG_HS_ULPI_DIR pins - How to uderstand this?

mikroforma
Associate II
Posted on July 26, 2012 at 21:27

Hi,

Has anybody seen that STM32F20x devices in 176pin packages has two  OTG_HS_ULPI_DIR pins at a same time:  at PI11 and PC2. 

How to understand this? If I enable ULPI and connect it to PI11 - what will be with PC2?

Can find anything about this in Datasheet or in Ref Manual.

The same story with OTG_HS_ULPI_NXT : it is doubled on PC3 and PH4.

Are they shorted together internally?

#usb-otg-hs-ulpi
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on July 26, 2012 at 22:01

You have to multiplex (mux) the pins out appropriately, you'd want to select only ONE routing. I'm sure you could configure the part to do stupid things, as a designer this is something you'll want to avoid. The a multiple escape pins to allow for peripherals and board routing concerns, and for the range of packages the same die can be bonded into.

Refer to Table 8 ''Alternate function mapping'' (pg 58) in the STM32F405xx/407xx manual.

http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/DATASHEET/DM00037051.pdf

For each pin row, pick one AF (Alternate Function) or be a GPIO

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mikroforma
Associate II
Posted on July 26, 2012 at 22:45

Ok, clear. Found - ref manual page 149 explained that

Thanks a lot