cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F2 USB HS-Core VCP Win7 not working

sw2sugar
Associate
Posted on January 21, 2013 at 04:00

Dear All.

I use STM32F205RCT6 and want to use VCP of USB HS-Core (PB13-15) with embedded PHY.

I wanted to use FS-Core (PA11-12) because I did and succeeded already.

But 64pin device doesn't include FS-Core.

I use VCP project of USB_Device_Examples in UsbLib V2.1.0.

Descripters (VID,PID,SERIAL etc)  are not changed (0x0483,0x5740,...).

Then run the STM32, Connect to the WinXP 32bit by USB Cable.

Failure the Device installation at first.

But executing VCP_V1.3.1_Setup.exe installs driver,

finally ' STMicroelectronics Virtual COM Port (COMxx) ' was appeared in Device manager without any warning.

It can Open , Close , Tx , Rx , everything OK.

Next , Connect to Win7 32bit by USB Cable,

Failure the Device Installation at first.

But executing VCP_V1.3.1_Setup.exe installs driver,

finally ' STMicroelectronics Virtual COM Port (COMxx) ' was appeared in Device manager but with yellow warning (code 10).

It can not Open the 'warning' port...

Followings are declared in the project.

USE_STDPERIPH_DRIVER

USE_USB_OTG_HS

USE_EMBEDDED_PHY

Is it need to change the INF file FS-Core and HS-Core ?

Could any one solve this ?

Thanks
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
sw2sugar
Associate
Posted on March 13, 2013 at 06:59

Dear All.

Can I ask following again ?

* CPU : STM32F205RCT6

* Module : USB HS-Core (PB13-15) with embedded PHY.

* Software : Virtual Comm Port of UsbLib V2.1.0.

* OS : Windows 7 32bit

* USB Driver : VCP_V1.3.1_Setup.exe

My result is that ' STMicroelectronics Virtual COM Port (COMxx) ' appears in Device manager WITH yellow warning (code 10).

I can not open this port.

Does anyone work well same as my condition ?

Thanks

bigdigital
Associate
Posted on April 04, 2013 at 11:01

I solve this problem by changingCDC_IN_FRAME_INTERVAL to 0 in usbd_conf.h , and now all work fine. Also i use this fix

https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/DispForm.aspx?ID=24294