Skip to main content
morpeh89
Associate III
December 27, 2012
Question

STM32F107 Virtual Com example - echo needed

  • December 27, 2012
  • 0 replies
  • 425 views
Posted on December 27, 2012 at 09:59

Hi!

I have a problem with usage of ST-example for Virtual Com port. I have STM32F107 on my board. Example is downloaded correctly and all seems workable. The thing is that my board is not standard evaluation board and it doesn't use USART. So, I decided to change example code to make it work without USART - only with USB.

I'd lile to make Echo-program: device should return back all bytes, received from PC.

In the code I see sevearl places, where data is sended or received from USB:

1. EP1_IN_Callback (void)

2. EP3_OUT_Callback(void)

3. Handle_USBAsynchXfer (void)

Two moments need clarification:

1. in EP3_OUT_Callback(void) i retranslate data, received from USB on EP3 to USB on EP1 instead of USART. Is it correct way?

... 

  USB_Rx_Cnt = USB_SIL_Read(EP3_OUT, USB_Rx_Buffer);

  USB_SIL_Write(EP1_IN, USB_Rx_Buffer, USB_Rx_Cnt);

  SetEPTxValid(ENDP1);

 ...

2. The problem I encounter here, is that program crashes any time after usage of USB_SIL_Write, cycling in the HardFault_Handler function. What can be reason of it?

It would be great if anyone gives me any advices concerning this points.

Thanks in advance!
    This topic has been closed for replies.