cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F105RB can1 and can2 model

ann Qian
Associate
Posted on June 02, 2018 at 06:35

Set can model Init setting in STM32CubeBx,and generate Code in keil5 project ,and then set Filter of can1 and can2 ,two of can 's transmation is OK,but receive is not;

Code as this:

CAN_FilterConfTypeDef FilterConfig;

CanTxMsgTypeDef TxMsg;

CanRxMsgTypeDef RxMsg;

 FilterConfig.FilterIdHigh = 0;

  FilterConfig.FilterIdLow = 0;

  FilterConfig.FilterMaskIdHigh = 0;

  FilterConfig.FilterMode =0;

  FilterConfig.FilterNumber=0;

  FilterConfig.FilterScale= CAN_FILTERSCALE_32BIT;

  FilterConfig.FilterFIFOAssignment= CAN_FILTER_FIFO0;

  FilterConfig.BankNumber= 0U;

  FilterConfig.FilterActivation= ENABLE;

  HAL_CAN_ConfigFilter(&hcan1, &FilterConfig);

  FilterConfig.BankNumber= 14U;

  FilterConfig.FilterFIFOAssignment= CAN_FILTER_FIFO1;

  HAL_CAN_ConfigFilter(&hcan2, &FilterConfig);

  for(;i<8;i++)

  TxMsg.Data[i] = i+1;

  TxMsg.DLC = 8;

  TxMsg.IDE = CAN_ID_EXT;

  TxMsg.ExtId = 0x02222222;

  TxMsg.RTR= CAN_RTR_DATA;

  hcan2.pTxMsg = &TxMsg;

  hcan2.pRx1Msg = &RxMsg;

 void main

{

       HAL_CAN_Receive(&hcan1, CAN_FIFO0,10);

       HAL_CAN_Receive(&hcan2, CAN_FIFO1,10);

}

register RF0R.FMP1   and RF1R.FMP1  when receive would be more than 0

and why?

thanks !!!

#stm32f105rb-can
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0