cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103ZE temperature sensor

Patel.Pritesh
Associate II
Posted on August 18, 2010 at 19:32

STM32F103ZE temperature sensor

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
John F.
Senior
Posted on May 17, 2011 at 14:03

It depends on your ADC range and variation in the temperature sensor characteristics. You can find out about the sensor in the datasheet.

http://www.st.com/stonline/products/literature/ds/14611/stm32f103ze.pdf

section 5.3.20

You'll see that the voltage out at 25C is typically 1.43V but it might be as low as 1.34V or as high as 1.52V. The variation with temperature (slope) varies too. All together it means you have to calibrate the sensor for each different microcontroller you get.

There are lots of better temperature sensors with I2C etc. interfaces or you can use a thermistor / resistor but watch out for the ADC input impedance requirements then.

greg_t
Associate II
Posted on May 17, 2011 at 14:03

The temperature sensor in the chip will measure the temperatue of the chip - if you need ambient tempeature use external sensor