cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103VCT6 USB Communication Port disconnection Problem Sometimes.

mohan raj
Associate II
Posted on July 12, 2018 at 08:48

Hi,

I am using STM32F103VCT6 for my project and I have Polling the data packets from Uc for every 200 milliseconds and send to PC,Sometimes USB Communication is disconnected.

when I debugging and find that Transmit state is set to one.afterwards USB port is disconnected,

is any solution to reconnect the USB port when the port is in disconnected state.

uint8_t CDC_Transmit_FS(uint8_t* Buf, uint16_t Len)

{

uint8_t result = USBD_OK;

/* USER CODE BEGIN 7 */

USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef*)hUsbDeviceFS.pClassData;

if (hcdc->TxState != 0){ -------> always Set to One.

return USBD_BUSY;

}

USBD_CDC_SetTxBuffer(&hUsbDeviceFS, Buf, Len);

result = USBD_CDC_TransmitPacket(&hUsbDeviceFS);

/* USER CODE END 7 */

return result;

}
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0