2019-09-24 2:22 AM
Hello.please may i have your help?
I have the error on the final part of debug launching only when i declare
const uint16_t __attribute__((section (".UserDataSector"))) out_val_register[64];//= {0x1234,0x1235,0x1238,0x3333};in .ld file
/* Specify the memory areas */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 20K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 124K
USER_DATA_FLASH (rx) : ORIGIN = 0x801F000, LENGTH = 4K
}
/* Define output sections */
SECTIONS
{
. = ALIGN(64);
/* placing my named section at given address: */
.my_block 0x801F000 :
{
KEEP(*(.UserDataSector)) /* keep my variable even if not referenced */
} > USER_DATA_FLASH
}
On other projects with smaller ST processor and same compiler i never had the same error doing the same things.
Any help will be appreciated.
Thanks,
Diego,
Milan,Italy,