cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103C8 Peripheral Alternate Function

markbell9
Associate II
Posted on June 14, 2012 at 15:55

On the STM32F103C8 chip I can use the PA9 default alternate function to use either USART1_TX or TIM1_CH2 on that pin depending upon which peripheral is enabled.

If both peripherals are enabled and I am using PA9 as USART1_TX, does this preclude me from using TIM_CH1, TIM_CH3, or TIM_CH4?

  

This assumes that TIM_CH2 is disabled:

TIM1 MOE =1

OSSR = x

CC2E = 0

CC2NE = 0

I pretty sure the answer is ''Yes'', but would like confirmation.

Thank you.

#stm32
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
raptorhal2
Lead
Posted on June 14, 2012 at 16:34

Each pin is independent as to alternate function, so the other timer channels are available.

Cheers, Hal

Andrew Neil
Super User
Posted on June 14, 2012 at 19:43

Many Alternate Functions can be ''re-mapped'' onto different pins...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Posted on June 14, 2012 at 20:04

Many Alternate Functions can be ''re-mapped'' onto different pins...

And sometimes must be otherwise pins clash. This is the case for one of the CAN outputs and a USART CTS or RTS pin. It's in the errata now, but banged my head on it with a 103 design. You need to remap the CAN off in the weeds. PA11 or PA12 as I recall.

Definitely review the errata as you floor plan the pin escape of your design.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..