cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103 Flash Firmware by Uart (Programming by Uart)

valeriogiampa
Associate II
Posted on April 28, 2011 at 10:46

STM32F103 Flash Firmware by Uart (Programming by Uart)

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
cschumann
Associate II
Posted on May 17, 2011 at 14:33

Hi Valerio,

How to flash software into the STM32 is described in the Application Notes

  • AN2606: System boot mode (http://www.st.com/stonline/books/pdf/docs/13801.pdf) and
  • AN3155: USART protocol (http://www.st.com/stonline/products/literature/an/17066.pdf)

There you can find the full protocol specification for the USART bootloader.

There is also a ''Flash loader demonstrator'' available which is capable of flashing a STM32 using UART.

Best regards,

Carsten Schumann

rrollet9
Associate II
Posted on May 17, 2011 at 14:33

1. Yes

2. I use this one under linux: 

http://code.google.com/p/stm32flash/

 Seems to be possible to run it under Windows

http://code.google.com/p/stm32flash/

3. Additional instructions available here: 

http://stm32.spacevs.com/