2024-05-16 2:57 AM
Hello,
I use the ADC1 with 5 channels in scan mode to obsurve different voltages.
Is it possible to define different AnalogWDGConfig.HighThreshold values for the channels?
Thanks,
Birgit
2024-05-16 4:46 AM
Hello @BBurg,
Unfortunately, Analog Watchdog is linked to ADC instance and could be configure for a single channel only or all channels in the same time.
There is probably a way to change the High Threshold on-the-fly based on DMA triggered by ADC but it has to be tested and timing can be a constraint.
I could have a look on this proposal.
Best Regards,
Gwénolé