cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f100c8 SPI & SST25VF016B read/write operation

rasimoguzturk
Associate III
Posted on October 13, 2012 at 18:39

hi all,i am working on external flash memory and stm32f100c8 communication via SPI,but in my code there is a wrong what i missed.perhaps you may see..

/*---------------------------------*/

#include ''stm32f10x.h''

#include ''stm32f10x_spi.h''

#include ''sFlash.h'' //sst25vf016b drivers

/*-------------------------------------------------------------*/

#define  FLASH_WriteAddress     0x700000 //flash memory address

#define  FLASH_ReadAddress      FLASH_WriteAddress

#define  FLASH_SectorToErase    FLASH_WriteAddress

#define  BufferSize (countof(Tx_Buffer)-1)

#define countof(a) (sizeof(a) / sizeof(*(a)))

uint8_t Tx_Buffer[] = ''HELLO'';//data to given memory address

uint8_t  Rx_Buffer[BufferSize];//read from given memory address

/*---------------------------------*/

/*---------------------------------*/

/*function prototypes*/

void RCC_Configuration(void);

void GPIO_Configuration(void);

void SPI_Configuration(void);

/*---------------------------------*/

/*---------------------------------*/

void RCC_Configuration(void)

{

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);

RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);

}

/*---------------------------------*/

/*---------------------------------*/

void GPIO_Configuration(void)

{

    GPIO_InitTypeDef GPIO_InitStructure;

//sck-5

//mosi 7

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5|GPIO_Pin_7;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; //out pushpull

GPIO_Init(GPIOA, &GPIO_InitStructure);

//nss 4 chip select

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; //out pushpull

GPIO_Init(GPIOA, &GPIO_InitStructure);

//miso 6

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;//In floating

GPIO_Init(GPIOA, &GPIO_InitStructure);

}

/*---------------------------------*/

/*---------------------------------*/

void SPI_Configuration(void){

SPI_InitTypeDef SPI_InitStructure;

GPIO_ResetBits(GPIOA,GPIO_Pin_5);

sFLASH_CS_HIGH();

SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;

SPI_InitStructure.SPI_Mode = SPI_Mode_Master;

SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;

SPI_InitStructure.SPI_CPOL = SPI_CPOL_High;

SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge;

SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;

SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2;

SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;

SPI_InitStructure.SPI_CRCPolynomial = 7;

  

SPI_Init(SPI1, &SPI_InitStructure);

SPI_Cmd(SPI1, ENABLE);

}

/*---------------------------------*/

/*---------------------------------*/

int main(){

RCC_Configuration();

GPIO_Configuration();

SPI_Configuration();

/*erase chip*/

    sFLASH_EraseBulk();

/*write tx buffer to Address with size*/

    sFLASH_WriteBuffer(Tx_Buffer, FLASH_WriteAddress, BufferSize);

/*read buffer from given memory address*/

    sFLASH_ReadBuffer(Rx_Buffer, FLASH_ReadAddress, BufferSize);

while(1);

}

when i write ''hello'' in TX,i see a strange char ''

ÿ

''(dec 255-hex 0xFF) in RX buffer.But normally should ''hello''..

thanks.

 
This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Posted on October 13, 2012 at 20:05

So it sounds like it reads back blank/erased memory.

Perhaps you need to disable block/write protection, or check the data sheet if there is some magic settings you need to send to initialize or unlock.

Check things like the chip ID, make sure that works, and is correct.

Check the status register, see if that looks valid, and check the block and write protection settings reported.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
rasimoguzturk
Associate III
Posted on October 14, 2012 at 12:21

thanks for suggestions clive,i will try them

rasimoguzturk
Associate III
Posted on October 17, 2012 at 19:22

hi clive,i tried suggestions,i read the Flash ID it has no problem but this time i can only read ''H'' of ''HELLO'' th others are ''FF'' i mean 

''

ÿ.

i guess i am writing only ''H'' of ''HELLO'' to memory.do you have any idea why is that..here is my updated code..:

#define  FLASH_WriteAddress     0x700000 //flash memory address

#define  FLASH_ReadAddress      FLASH_WriteAddress

#define  FLASH_SectorToErase    FLASH_WriteAddress

#define  sFLASH_ID       0x00BF2541 //flash ID for sst25 16mbit family

/*-------------------------------------------------------------*/

/*-------------------------------------------------------------*/

#define   BufferSize (countof(Tx_Buffer)-1)

#define countof(a) (sizeof(a) / sizeof(*(a)))

/*-------------------------------------------------------------*/

/*-------------------------------------------------------------*/

uint8_t Tx_Buffer[] = ''HELLO''; //data to given memory address

uint8_t  Rx_Buffer[BufferSize]; //read from given memory address

__IO uint32_t FlashID=0;

/*---------------------------------*/

/*---------------------------------*/

/*function prototypes*/

void RCC_Configuration(void);

void GPIO_Configuration(void);

void SPI_Configuration(void);

void EWSR(void); //enable write status register

void WRSR(uint8_t byte);

/*---------------------------------*/

/*---------------------------------*/

void RCC_Configuration(void)

{

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);

RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE);

}

/*---------------------------------*/

/*---------------------------------*/

void GPIO_Configuration(void)

{

    GPIO_InitTypeDef GPIO_InitStructure;

//sck pin 5-mosi pin 7

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5|GPIO_Pin_7;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; //out pushpull

GPIO_Init(GPIOA, &GPIO_InitStructure);

//nss pin(CS) 4 chip select

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; //out pushpull

GPIO_Init(GPIOA, &GPIO_InitStructure);

//miso pin 6

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;//In floating

GPIO_Init(GPIOA, &GPIO_InitStructure);

//led

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_14;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; //out pushpull

GPIO_Init(GPIOB, &GPIO_InitStructure);

}

/*---------------------------------*/

/*---------------------------------*/

void SPI_Configuration(void){

SPI_InitTypeDef SPI_InitStructure;

sFLASH_CS_HIGH(); //Deselect flash-chip select pin high

SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;

SPI_InitStructure.SPI_Mode = SPI_Mode_Master;

SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;

SPI_InitStructure.SPI_CPOL = SPI_CPOL_High;

SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge;

SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;

SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2;

SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;

SPI_InitStructure.SPI_CRCPolynomial = 7;

  

SPI_Init(SPI1, &SPI_InitStructure);

SPI_Cmd(SPI1, ENABLE);

}

/*---------------------------------*/

/*---------------------------------*/

int main(){

long int i;

RCC_Configuration();

GPIO_Configuration();

SPI_Configuration();

FlashID = sFLASH_ReadID(); //get Flash ID

if(FlashID==sFLASH_ID){ //if flash ID matches do operation

GPIO_SetBits(GPIOB, GPIO_Pin_14); //blink led until op.complete

EWSR();

WRSR(0x00);

/*erase sector chip*/

sFLASH_EraseSector(FLASH_SectorToErase);

/*write tx buffer to Address with size*/

sFLASH_WriteBuffer(Tx_Buffer, FLASH_WriteAddress, BufferSize);

/*read buffer from given memory address*/

sFLASH_ReadBuffer(Rx_Buffer, FLASH_ReadAddress, BufferSize);

for(i=0;i<10000000;i++);

GPIO_ResetBits(GPIOB, GPIO_Pin_14); //led off

}

while(1);

}

 

rasimoguzturk
Associate III
Posted on October 17, 2012 at 19:27

to be migrated, sourceId: 25556:697285D7-A9CA-445D-B16C-F23BF0E3B1A3

Posted on October 17, 2012 at 21:17

Absent HW I can't really assist you.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
cagdasyet
Associate
Posted on June 24, 2015 at 15:06

You can not write multiple adress witout

Auto Address Increment (AAI) Word-Program Sequence

This is the code

/************************************************************************/

/* PROCEDURE: WRDI                            */

/************************************************************************/

void WRDI()

{

    sFLASH_CS_LOW();            /* enable device */

    YYCM_SpiPut(0x04);        /* send WRDI command */

    sFLASH_CS_HIGH();            /* disable device */

}

/************************************************************************/

/* PROCEDURE:    Auto_Add_IncA                        */

//------Dikkat Sadece 2 nin katlari seklinde yazabiliyor AUTO increment

// Auto Address Increment (AAI) Word-Program Sequence with Software End-of-Write Detection

/************************************************************************/

void sFLASH_WritePage_AutoINC(uint8_t* pBuffer,unsigned long Dst,uint16_t NumByteToWrite)

{

    //EBSY();     /* Enable SO as RY/BY# output if in AAI */

    sFLASH_WriteEnable();

    

    sFLASH_CS_LOW();                /* enable device */

    YYCM_SpiPut(0xAD);            /* send AAI command */

    YYCM_SpiPut(((Dst & 0xFFFFFF) >> 16));     /* send 3 address bytes */

    YYCM_SpiPut(((Dst & 0xFFFF) >> 8));

    YYCM_SpiPut(Dst & 0xFF);

    YYCM_SpiPut(*pBuffer);            /* send 1st byte to be programmed */

    pBuffer++;    

    YYCM_SpiPut(*pBuffer);            /* send 2nd byte to be programmed */

    pBuffer++;

    sFLASH_CS_HIGH();                /* disable device */

    

    NumByteToWrite=NumByteToWrite-2;

    

    while (NumByteToWrite) //!!!Dikkat Bu Sekilde Calismiyor  Otomatik Aderss artt1rma vs yok!!!

  {

        sFLASH_CS_LOW();                /* enable device */

        YYCM_SpiPut(0xAD);            /* send AAI command */

        YYCM_SpiPut(*pBuffer);            /* send 1st byte to be programmed */

        pBuffer++;

        YYCM_SpiPut(*pBuffer);            /* send 2nd byte to be programmed */

        pBuffer++;

        sFLASH_CS_HIGH();                /* disable device */

        NumByteToWrite=NumByteToWrite-2;

    }

    

    WRDI();                 /* Exit AAI before executing DBSY */

    //DBSY();                    /* disable SO as RY/BY# output if in AAI */

    sFLASH_WaitForWriteEnd();

}