Question
stm32F100 RX
Posted on March 20, 2012 at 17:28
hi can any one help me this code seems to be right but i dont know what' the matter with Rx FAILED LED turn always on !!!???
#include ''stm32f10x.h''#include ''stm32f10x_rcc.h''#include ''stm32f10x_usart.h'' #include ''stm32f10x_gpio.h''uint8_t ch;// pour USART1 PA9 et PA10, pour USART2 PA2 et PA3#define RCC_APB2Periph_GPIOx RCC_APB2Periph_GPIOA#define GPIO_Pin_Tx1 GPIO_Pin_9 // PA9 sortie#define GPIO_Pin_Rx1 GPIO_Pin_10 // PA10 entree#define GPIO_Pin_Tx2 GPIO_Pin_2 // PA2 sortie#define GPIO_Pin_Rx2 GPIO_Pin_3 // PA3 entreetypedef enum { FAILED = 0, PASSED = !FAILED} TestStatus;#define countof(a) (sizeof(a) / sizeof(*(a)))#define TxBufferSize countof(TxBuffer)GPIO_InitTypeDef GPIO_InitStructure;TestStatus TransferStatus = FAILED; ErrorStatus HSEStartUpStatus;/* Private variables ---------------------------------------------------------*/USART_InitTypeDef USART_InitStructure;u8 TxBuffer[] = ''a1a34 ceci est un essai'';u8 RxBuffer[TxBufferSize];u8 TxCounter = 0, RxCounter = 0; /* Private function prototypes -----------------------------------------------*/void RCC_Configuration(void); // configuration horloge PortA et horloge Usartvoid GPIO_Configuration(void); // configuration pattes entrees/sortiesvoid NVIC_Configuration(void); // configuration interruption (ici non utilisee)TestStatus Buffercmp(u8* pBuffer1, u8* pBuffer2, u16 BufferLength);//u8 index = 0;void GPIO_Configuration(void){ GPIO_InitTypeDef GPIO_InitStructure;#ifdef USE_STM3210B_EVAL /* Enable the USARTx Pins Software Remapping */ GPIO_PinRemapConfig(GPIO_Remap_USART1, ENABLE); GPIO_PinRemapConfig(GPIO_Remap_USART2, ENABLE);#endif /* Configure USART1 Tx (PA.09) as alternate function push-pull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_Tx1; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); // Tx USART1 en sortie push pull /* Configure led as alternate function push-pull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_8; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(GPIOC, &GPIO_InitStructure); /* Configure USART2 Tx as alternate function push-pull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_Tx1; //PIO_Init(GPIOA, &GPIO_InitStructure); // configurer Tx USART2 en sortie push pull GPIO_Init(GPIOA, &GPIO_InitStructure); /* Configure USART1 Rx (PA.10) as input floating */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_Rx1; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &GPIO_InitStructure); // configurer Rx USART1 en entree flottante /* Configure USART2 Rx as input floating */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_Rx2; GPIO_Init(GPIOA, &GPIO_InitStructure); // configurer Rx USART2 en entree flottante}TestStatus Buffercmp(u8* pBuffer1, u8* pBuffer2, u16 BufferLength){ while(BufferLength--) { if(*pBuffer1 != *pBuffer2) { return FAILED; } pBuffer1++; pBuffer2++; } return PASSED; }int main(void){ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); // autorise GPIO RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); // autorise USART1 RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE); // autorise USART2 SystemInit(); // initialiser horloge et PLLMUL systeme et USART // GPIO_Configuration(); // configuration GPIO USART_InitStructure.USART_BaudRate = 115200; // configuration vitesse USART_InitStructure.USART_WordLength = USART_WordLength_8b; // configuration longueur mot USART_InitStructure.USART_StopBits = USART_StopBits_1; // bit de stop USART_InitStructure.USART_Parity = USART_Parity_No; // bit de parite USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; // hardware control USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; // half duplex /* Configure USART1 */ USART_Init(USART1, &USART_InitStructure); // initialisation registres internes (SR et BRR) USART1 /* Configure USART2 */ USART_Init(USART2, &USART_InitStructure); // initialisation registres internes (SR et BRR) USART2 USART_Cmd(USART1, ENABLE); // autoriser USART1 a fonctionner /* Enable the USART2 */ USART_Cmd(USART2, ENABLE); // autoriser USART2 a fonctionner while(TxCounter < TxBufferSize) { /* envoyer un caractere de USART1 a USART2 */ ch=TxBuffer[TxCounter++]; if (ch=='c'){GPIO_SetBits(GPIOC,GPIO_Pin_9);}while (!(USART1->SR & USART_FLAG_TXE)); // tester si registre a decalge vide (Bit TXE) registre SRUSART1->DR = ch; // envoyer caractere pareil que USART_SendData(USART1, TxBuffer[TxCounter++]);// USART1->DR = (ch1 & (uint16_t)0x01FF); while(USART_GetFlagStatus(USART2, USART_FLAG_RXNE) == RESET) { } /* Store the received byte in RxBuffer */ RxBuffer[RxCounter++] = (USART_ReceiveData(USART2) & 0x7F); // why we must ''&'' the received value with 0x7F!!!!! if (RxBuffer[RxCounter -1]=='c'){GPIO_SetBits(GPIOC,GPIO_Pin_8);} } /* Check the received data with the send ones */ TransferStatus = Buffercmp(TxBuffer, RxBuffer, TxBufferSize); if (TransferStatus== PASSED) {GPIO_SetBits(GPIOC,GPIO_Pin_8); } } // si le contenu des deux buffers de reception et d'emission sont identiques c'est que //la communication entre port serie 1USART1 et port serie 2 USART1 s'est bien faite: PASS = 1, Failed = 0