Stm32f051 adc for multiple channels
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-04-07 12:14 AM
Hello everyone,
I have problem with the ad conversion into the stm32f051 microcontroller. My Destination is: AD-convert for multiple channels PC0, PC1, PC2, PC3, PB0 und PB1 My Problem:The
AD values
do not match the
voltage values at
the respective channel
My Code:// Initalization Reset and clock control (RCC)
void init_RCC(void)
{
/* GPIO Ports and DMA1 Clock avtivate */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA
| RCC_AHBPeriph_GPIOB
| RCC_AHBPeriph_GPIOC
| RCC_AHBPeriph_GPIOD, ENABLE);
/* SPI1 and SPI2 Clock activate */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);
/* USART clock activate */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);
/* TIM14 clock activate */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM14, ENABLE);
/* ADC clock activate */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
}
void init_ADC()
{
/* Structure definition GPIO_InitStruct at GPIO_initTypDef */
GPIO_InitTypeDef GPIO_InitStruct;
/* Structure definition ADC_InitStruct at ADC_initTypDef */
ADC_InitTypeDef ADC_InitStruct;
/* Configure ADC pins : PC0, PC1, PC2, PC3 */
GPIO_InitStruct.GPIO_Pin = GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_3;
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStruct.GPIO_Speed = GPIO_Speed_Level_1;
GPIO_Init(GPIOC, &GPIO_InitStruct);
/* Configure ADC pins : PB0, PB1 */
GPIO_InitStruct.GPIO_Pin = GPIO_Pin_0|GPIO_Pin_1;
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStruct.GPIO_Speed = GPIO_Speed_Level_1;
GPIO_Init(GPIOB, &GPIO_InitStruct);
/* Put everythink back to power-on defaults */
ADC_DeInit(ADC1);
/* Initalize ADC structure */
ADC_StructInit(&ADC_InitStruct);
/* ADC-Structure initialization */
ADC_InitStruct.ADC_ContinuousConvMode = DISABLE; /* After the end of conversion, the next conversion will be started automatically if ENABLE */
ADC_InitStruct.ADC_DataAlign = ADC_DataAlign_Right; /* Data align into the right from LSB */
ADC_InitStruct.ADC_ExternalTrigConv = ADC_ExternalTrigConvEdge_None; /* Data with not external trigger configuration */
ADC_InitStruct.ADC_Resolution = ADC_Resolution_12b; /* ADC resolution from 12 Bit */
ADC_InitStruct.ADC_ScanDirection = ADC_ScanDirection_Upward; /* ADC scans the channel upward */
ADC_Init(ADC1, &ADC_InitStruct); /* ADC1 initalize with configuration parameters */
/* Aktivate ADC */
ADC_Cmd(ADC1, ENABLE);
}
uint16_t readADC1(uint8_t channel)
{
/* Activate ADC1 in coninous mode */
//ADC_DiscModeCmd(ADC1, ENABLE);
/* Channel configuration */
ADC_ChannelConfig(ADC1, channel, ADC_SampleTime_1_5Cycles);
/* Start the conversion */
ADC_StartOfConversion(ADC1);
/* Wait until conversion completion */
while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC));
/* Get the conversion value */
uint16_t Value = ADC_GetConversionValue(ADC1);
/* Clear EOC Flag */
ADC_ClearFlag(ADC1, ADC_FLAG_EOC);
return Value;
}
int main(void)
{
init_RCC(); /* Reset and Clock Control initialized */
init_GPIO(); /* General Purpose Inputs- and Outputs initialized */
if (SysTick_Config(SystemCoreClock / reloadValueDiv))
{
/* Capture error */
while (1);
}
init_SPI(); /* Serial Peripheral Interface initialized */
//init_USART(); /* Universal Synchronous and Asynchronous Receiver Transmitter initialized */
init_NVIC(); /* Nested Vectored Interrupt Controller initialized */
//init_Timer(); /* Timer initialized */
GPIO_WriteBit(GPIOB, GPIO_Pin_2, Bit_SET); /* ADC_RESET = nRESET set high */
init_ADS8332(ads8332_configuration_setting); /* ADS8332 Initialized with ads8332_configuration_setting*/
if((get_ADS8332_configuration() & 0x0FFF) != (ads8332_configuration_setting & 0x0FFF)) /* If the receive ads8332 configuration is not equal, than capture error. */
{
/* Capture error */
while (1);
}
GPIO_WriteBit(GPIOB, GPIO_Pin_6, Bit_SET); /* ADC_CS = nCS set high */
GPIO_WriteBit(GPIOB, GPIO_Pin_12, Bit_SET); /* nCONVST = nCS set high */
init_ADC(); /* ADC initialized */
while (1)
{
GPIO_WriteBit(GPIOA, GPIO_Pin_5, Bit_SET);
for(i=0;i<8;i++){
spiDataBufferSPI1[i] = get_ADS8332_adc_value(i);
}
for(j=0;j<6;j++){
value[j] = readADC1(j);
}
/* Wait rest cycle time in this delay-function */
Delay(CYCLE_TIME);
GPIO_WriteBit(GPIOA, GPIO_Pin_5, Bit_RESET);
}
}
Please help me,
I
'm new to this
area
. Haak- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-04-07 11:17 AM
In the analog world, it helps to state how much error you are observing.
1.5 sample time might be too short if you don't have a low impedance signal source. Increase the sample time to the largest value available. If that fixes the problem, decrease the time to whatever still works. Cheers, Hal- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-04-07 11:15 PM
Hello Hal,
Thank you for
your
suggestion.
1
) I havethe ADC
Sample
Time
increased to
239.5
cycles and
start
the debug mode
.In the first
program cycle
following
AD
values
will be read
…Value[0] = 1053; // The correct
values
should be
2110
decimal
Value[1] = 0; // and
all other values
would
also have a
small offset
Value[2] = 0;
Value[3] = 0;
Value[4] = 0;
Value[5] = 0;
and
in the second and
higher
program
cycles
following
values are read
...
Value[0] = 0; // The correct
values
should be
2110
decimal
Value[1] = 0; // and
all other values
would
also have a
small offset
Value[2] = 0;
Value[3] = 0;
Value[4] = 0;
Value[5] = 0;
2)
I havethe ADC
Sample
Time
increased to
55.5
cycles and
start
the debug mode
.In the first
program cycle
following
AD
values
will be read
…Value[0] = 1054; // The correct
values
should be
2110
decimal
Value[1] = 285; // and
all other values
would
also have a
small offset
Value[2] = 45;
Value[3] = 37;
Value[4] = 31;
Value[5] = 93;
and
in the second and
higher
program
cycles
following
values are read
...
Value[0] = 218; // The correct
values
should be
2110
decimal
Value[1] = 110; // and
all other values
would
also have a
small offset
Value[2] = 104;
Value[3] = 104;
Value[4] = 103;
Value[5] = 108;
It seems
as if the
AD
values do not
change with
changing
external
voltage
. I have pulled the voltage to ground on the PC 0 AD input and received the same value as described above.Can
someone tell me if
my
ADC
Configuration and readADC1()-function
is correct
?
I want to
read the
analog
channels
PC0, PC1, PC2, PC3, PB0 and PB1.
Best regards
Haak
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-04-08 6:50 AM
I am not familiar with the F05, but comparing the code with the data sheet pinout table, it looks like you are trying to convert ADC channels 0 to 5 but set up GPIO pins in analog mode for channels 10 to 13 (PC0 to PC3) and 8 & 9 (PB0 & PB1).
Cheers, Hal- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-04-08 4:43 PM
I presume you are examining your options at this point.
Multiple ADC channel conversions are usually saved in a buffer using DMA, rather than reading the ADC conversion register after each conversion. See the Reference Manual and ADC examples on how to do this. You posted in an Evaluation Tools forum. If you are using a Discovery or Evaluation board, refer to the board's User Manual to ensure the pins are free for your use. Cheers, Hal