cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F042 MEM_MODE problem

x8932
Associate II
Posted on September 30, 2015 at 16:59

Hello,

i use STM32F042C6 MCU and change SYSCFG MEM_MODE to 1 (System Flash memory mapped at 0x00000000) but always see Main Flash (0x08000000) data from address 0x00000000.

Also i try set 11 (Embedded SRAM mapped at 0x00000000) but unsuccess.

Also i try jump to system bootloader (0x1FFFC400) but MCU back to 0x08000000 vector after small delay (with USB connected).

Can anybody use software jump to system bootloader ?

#stm32f0
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on September 30, 2015 at 17:25

Hi Mitek,

It seems that you haven't update the BOOT0 pin (it has to be set to 1).

Did you tried using the ST-Link Utility?

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.