cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F0308-DISCO stop consumption

r239955
Associate
Posted on May 20, 2014 at 15:03

Hi all.

I have to test stop comsunption using jumper JP2 present 

on th board (STM32F0308-DISCO board).

I have measured high value (abiut 200 uA)

Into STM32F030x datasheet the value is declared about 5 to 32 uA Max

Note that:

-All GPIO are OUT with no pull up - no pull down, at 0 level and with no loads connected

- Only PORTA is in input with push button B1 cpnnected

- All pheripheral, and CPU clock stopped

- Only LSI clock active to clock RTC

-1,8 Volts internal regulator is in low power modality

-A/D off

- The board is powered from PC usb interface

Thank's in advance for help

  Roberto

 
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0