STM32F030 standby mode cannot wakeup it
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-07-21 3:33 AM
Posted on July 21, 2016 at 12:33
Hello,
I want to try to wake up the F030 out of the standby mode. I enabled HAL_PWR_EnableWakeUpPin, then put the chip into low power mode with HAL_PWR_EnterSTANDBYMode. I know that to wake it up i should make a rising edge to it. I made a pushbutton to give a current to it. For an indication i use blinking LED that so i know if anything is moving, but upon standby mode the led lights up and doesn't come blink after i push the button that should wake up the PA0 pin. Can someone give any advice on what maybe I'm doing wrong or some info on where to move? Would be helpfull, thank you. #- #standby #pwr #stm32f030
Labels:
- Labels:
-
Power
-
STM32F0 Series
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-07-21 6:57 AM
Posted on July 21, 2016 at 15:57
Hi sutkus.rokas,
I suggest you to have a look to this example under the STM32F0 cube firmware package:STM32Cube_FW_F0_V1.6.0\Projects\STM32072B_EVAL\Examples\PWR\PWR_STANDBY It shows how to enter the system to STANDBY mode and wake-up from this mode using: external RESET, RTC Alarm A or WKUP pin.-Syrine-