cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F0 Unique ID Location

tderensis
Associate II
Posted on October 19, 2015 at 21:18

What is the starting address of the 96-bit Unique ID on the STM32F030 processors? I cannot find this information anywhere in the reference manual or datasheet. Is this guaranteed to exist on the F0 series?

#stm32f0 #unique-id
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on October 19, 2015 at 21:44

Some F0 parts do, the page for the

http://www.st.com/web/en/catalog/mmc/SC1169/SS1574/LN1826/PF258968

doesn't claim it has one, whereas the

http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1574/LN1447/PF253344?sc=internet/mcu/product/253344.jsp

does. Bottom of the ''Key Features'' list.

The absence in

http://www.st.com/web/en/resource/technical/document/reference_manual/DM00091010.pdf

Chap 27, also would seem to confirm that it's not present/supported in your chosen chip. Would appear to be a purposeful omission.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Amel NASRI
ST Employee
Posted on October 20, 2015 at 18:08

Hi derensis.thomas,

I confirm that the Unique ID isn't available for STM32F030x4/6/8/C and STM32F070x6/B (the ones covered by RM0360).

Please note that STM32F050 devices were renamed to STM32F031 (RM0091). Tha's why it supports the Unique ID feature.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.