cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F0 and HC 06

edouard
Associate II
Posted on September 01, 2015 at 12:03

Hello,

I am trying to send data to a computer with an HC 06 linked to an STM32F0 Discovery.

Here is my code :

 /* USART2 PA.2 Tx, PA.3 Rx STM32F0-Discovery*/

/* Includes ------------------------------------------------------------------*/

#include ''main.h''

#include ''stdio.h''

 

/* Private variables ---------------------------------------------------------*/

 

 

/* Functions prototypes ---------------------------------------------------------*/

void RCC_Configuration(void)

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); /*Activation des clocks de l'usart2 et du port A*/

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2,ENABLE);

}

 

void configUSART2 (void)

{

USART_InitTypeDef USART_InitStructure;

USART_InitStructure.USART_BaudRate = 9600;

  USART_InitStructure.USART_WordLength = USART_WordLength_8b;

  USART_InitStructure.USART_StopBits = USART_StopBits_1;

  USART_InitStructure.USART_Parity = USART_Parity_No;

  USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

  USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

  USART_Init(USART2, &USART_InitStructure);

USART_Cmd(USART2,ENABLE);

}

void configGPIOA (void)

{

GPIO_InitTypeDef GPIO_InitStructure;

GPIO_InitStructure.GPIO_Pin =  GPIO_Pin_2 | GPIO_Pin_3;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;

  GPIO_Init(GPIOA, &GPIO_InitStructure);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_1);

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_1);

}

void Usart2Send(uint8_t data)

{

      USART_SendData(USART2, (uint8_t) data);

      //Loop until the end of transmission

      while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET)// Wait for Empty

      {

      }

}

void outstring(char *s)

{

  while(*s)

  {

    /* Loop until transmit data register is empty */

    while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET)// Wait for Empty

 

    USART_SendData(USART2, (uint8_t)*s++);

  }

}

uint8_t Usart2Read(void){

     while ( USART_GetFlagStatus(USART1, USART_FLAG_RXNE) == RESET);

     return (uint8_t)USART_ReceiveData(USART2);

}

int main(void)

{

RCC_Configuration();

configUSART2();

configGPIOA();

Usart2Send('A');

Usart2Send('T');

  while(1)

  { 

  }

}

     

     

Here is what i get on Putty :

▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒

▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒AT▒▒▒▒▒

▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒n▒▒▒

▒▒▒▒▒▒▒▒▒▒▒▒Ǡ▒̸▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒

▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒l▒▒▒

▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒A

I configured on keil on putty the same parameters : 9600baud, 8 bits data, 1 bit stop, no parity and no verification.

Any idea ? (by the way, I did not find how to put my code properly on the forum, sorry about that).

Thanks in advance
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on September 01, 2015 at 18:17

The Format Code Block tools is the Paintbrush [<>] icon, top left of the Word-in-a-box(tm) interface.

The HC-06 might need configuring at the STM32 end, sending ''AT'' command (no CR/LF) and waiting is the way of getting into command mode, as I recall, not sure you'd get that data over the air once it switches out of data mode.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..