2014-04-23 6:46 AM
Has the USB framework supplied with STM32CubeF4 been completely rewritten or is it the USB-Host-Device_Lib_V2.1.0?
2014-04-24 12:48 AM
Why not do a compare of them with any common compare tool?
2014-04-24 2:38 AM
I do not think it is as simple as doing a compare.
1. (from what I understand) The Cube tool generates the code for the specified processor and environment (OS, IDE etc) 2. Since one generates code for specific processors and the other has to cater for a number of processors - one will contain compiler directive and the other will not. 2. Naming conventions are different between the 2We’re moving the ST Community to a new platform to give you a better and more reliable community experience.