cancel
Showing results for 
Search instead for 
Did you mean: 

STM32C071 SVD File

MBake.4
Associate II

Hello, I am in need of the SVD file for the newly released C071 model with USB. AFAICT they have not been posted or updated anywhere yet.

I'm working in Rust which requires the SVD file for generating register accessors so I cannot do anything with the chip until they are available.

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @MBake.4 

This file is published. you can download it from this link (the version 1.2 of the STM32C0 SVD file).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
STTwo-32
ST Employee

Hello @MBake.4 

This file is published. you can download it from this link (the version 1.2 of the STM32C0 SVD file).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you very much!

Guillaume K
ST Employee

Thanks for contributing on Rust for STM32C0 !

Thanks, I have now succeeded to establish USB Serial communications with C071 on the Rust/stm32-rs stack using the provided SVD files.