cancel
Showing results for 
Search instead for 
Did you mean: 

STM32C071 LQFP 32pin, need some help for first time design

LMore.2
Associate III

I've already become familiar with the NUCLEO-C071 by creating some additional hardware (display, encoder, etc.). Now, I want to design a board using the smaller 32-pin version. However, in this smaller version, I find some differences that I don't know how to address (I have read the datasheet thoroughly multiple times but cannot find any answers):

1) In the 64-pin version, pin 6 is the VBAT to connect a battery or a supercapacitor to maintain the RTC operation in case of power loss. Where has it gone in the 32-pin version?

2) In the 64-pin version, both the quartz for the CPU and for the RTC can be mounted. Can you confirm that in the 32-pin version, the CPU only works without quartz? Even for managing USB?

Thank you to anyone who can help me.

Luca.

11 REPLIES 11
LMore.2
Associate III

It certainly works, but I don't find this solution very efficient. However, I acknowledge that there is no other solution. Thank you.

Andrew Neil
Super User

On switching & detecting between "main" and "backup" power:

https://community.st.com/t5/stm32-mcus-products/micro-without-vbat-pin-detect-main-or-backup-power/td-p/769918

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.