cancel
Showing results for 
Search instead for 
Did you mean: 

STM3210VE, 8G SD card , SDIO 4bits bus, DMA mode-STOne-32,help me please

linkai1020
Associate II
Posted on September 17, 2010 at 03:07

STM3210VE, 8G SD card , SDIO 4bits bus, DMA mode-STOne-32,help me please

This discussion is locked. Please start a new topic to ask your question.
26 REPLIES 26
afinko
Associate II
Posted on May 17, 2011 at 14:07

Can you pleas attach the whole project, that works with such SD cards?

It would be very helpful.

Thanks in advance.

linkai1020
Associate II
Posted on May 17, 2011 at 14:07

420KB / S to write the file is too slow, I'm improving.

When writing the file the CPU is waiting for DMA, DMA can not play the greatest effectiveness.

I was to change the code, it will be updated here. 

Tomorrow is

China National Day

, I come back in 7 days.

Happy Holidays!

linkai1020
Associate II
Posted on May 17, 2011 at 14:07

      DMA_TxConfiguration(writebuff, (NumberOfBlocks * BlockSize));

      while ((DMA_GetFlagStatus(DMA2_FLAG_TC4) == RESET) && (DMA_GetFlagStatus(DMA2_FLAG_TE4) == RESET) && (TransferError == SD_OK)); // TransferError set by interrupt handler.

//--

Every time when configuring DMA, CPU in a wait state.

This is very bad you know.

fabrizio_dorazio
Associate II
Posted on May 17, 2011 at 14:07

please attach the whole project...I have same problem.....

Thanks...

linkai1020
Associate II
Posted on May 17, 2011 at 14:07

I rewrite the code,There are few

Changes

in the sdcard.c.

I try to attach the new project,but the Great Fire Wall......you know......

so.the changs below:

SD_Error SD_EnableWideBusOperation(u32 WideMode)

{

  SD_Error errorstatus = SD_OK;

  /* MMC Card doesn't support this feature */

  if (SDIO_MULTIMEDIA_CARD == CardType)

  {

    errorstatus = SD_UNSUPPORTED_FEATURE;

    return(errorstatus);

  }

  else if ((SDIO_STD_CAPACITY_SD_CARD_V1_1 == CardType) || (SDIO_STD_CAPACITY_SD_CARD_V2_0 == CardType) || (SDIO_HIGH_CAPACITY_SD_CARD == CardType))

  {

    if (SDIO_BusWide_8b == WideMode)

    {

      errorstatus = SD_UNSUPPORTED_FEATURE;

      return(errorstatus);

    }

    else if (SDIO_BusWide_4b == WideMode)

    {

      errorstatus = SDEnWideBus(ENABLE);

      if (SD_OK == errorstatus)

      {

        /* Configure the SDIO peripheral */

//        SDIO_InitStructure.SDIO_ClockDiv = SDIO_TRANSFER_CLK_DIV;

           

        SDIO_InitStructure.SDIO_ClockDiv = SDIO_TRANSFER_CLK_DIV + 9;//6M 

            

        SDIO_InitStructure.SDIO_ClockEdge = SDIO_ClockEdge_Rising;

        SDIO_InitStructure.SDIO_ClockBypass = SDIO_ClockBypass_Disable;

        SDIO_InitStructure.SDIO_ClockPowerSave = SDIO_ClockPowerSave_Disable;

  SDIO_InitStructure.SDIO_BusWide = SDIO_BusWide_4b;

//        SDIO_InitStructure.SDIO_HardwareFlowControl = SDIO_HardwareFlowControl_Disable;

        SDIO_InitStructure.SDIO_HardwareFlowControl = SDIO_HardwareFlowControl_Disable;

        SDIO_Init(&SDIO_InitStructure);

      }

    }

-----------------------------------------------------------------

SD_Error SD_WriteMultiBlocks(u32 addr, u32 *writebuff, u16 BlockSize, u32 NumberOfBlocks)

{

............................................

     DMA_TxConfiguration(writebuff, (NumberOfBlocks * BlockSize));

      while ((DMA_GetFlagStatus(DMA2_FLAG_TC4) == RESET) && (DMA_GetFlagStatus(DMA2_FLAG_TE4) == RESET) && (TransferError == SD_OK)); // TransferError set by interrupt handler.

      if (DMA_GetFlagStatus(DMA2_FLAG_TE4)==SET) TransferError = SD_ERROR;    //uart_puts(''DMA Transfer error\n'');   

      if (TransferError!=SD_OK) return(TransferError);

//      while (DMA_GetFlagStatus(DMA2_FLAG_TC4) == RESET)

//      {}

      while ((TransferEnd == 0) && (TransferError == SD_OK))

      {}

      if (TransferError != SD_OK)

      {

        return(TransferError);

      }

    }

  }

  /* Clear all the static flags */

  SDIO_ClearFlag(SDIO_STATIC_FLAGS);

  /* Wait till the card is in programming state *///�?等待flash擦写完毕

//  errorstatus = IsCardProgramming(&cardstate);

//

//  while ((errorstatus == SD_OK) && ((cardstate == SD_CARD_PROGRAMMING) || (cardstate == SD_CARD_RECEIVING)))

//  {

//    errorstatus = IsCardProgramming(&cardstate);

//  }

  return(errorstatus);

}

............................................

FRESULT f_write (

 FIL *fp,   /* Pointer to the file object */

 const void *buff, /* Pointer to the data to be written */

 UINT btw,   /* Number of bytes to write */

 UINT *bw   /* Pointer to number of bytes written */

)

...........................

 for ( ;  btw;         /* Repeat until all data transferred */

  wbuff += wcnt, fp->fptr += wcnt, *bw += wcnt, btw -= wcnt) {

  if ((fp->fptr % SS(fp->fs)) == 0) {   /* On the sector boundary? */

   if (fp->csect >= fp->fs->csize) {  /* On the cluster boundary? */

    if (fp->fptr == 0) {    /* On the top of the file? */

     clst = fp->org_clust;   /* Follow from the origin */

     if (clst == 0)     /* When there is no cluster chain, */

      fp->org_clust = clst = create_chain(fp->fs, 0); /* Create a new cluster chain */

    } else {       /* Middle or end of the file */

     clst = create_chain(fp->fs, fp->curr_clust);   /* Follow or streach cluster chain */

    }

    if (clst == 0) break;    /* Could not allocate a new cluster (disk full) */

    if (clst == 1) ABORT(fp->fs, FR_INT_ERR);

    if (clst == 0xFFFFFFFF) ABORT(fp->fs, FR_DISK_ERR);

    fp->curr_clust = clst;    /* Update current cluster */

    fp->csect = 0;      /* Reset sector address in the cluster */

   }

//before i am writting,i format the clusters to 32KB because i write less than 32KB one time

.........................

linkai1020
Associate II
Posted on May 17, 2011 at 14:07

There are much other codes in the whole project and it is b

elonging to the company,i'm sorry.

If you attach  your project,

I can fix it and test it in the t

he same environment

 for you.

Posted on May 17, 2011 at 14:07

Howdy

I'm using 4bit wide SDIO with DMA. I haven't encountered any problems with DMA, only SDIO CRC errors after writing. Increasing SDIO_TRANSFER_CLK_DIV by one solved the problem. I'm using the code from CMSIS 3.3.0 examples directory.