2015-07-14 6:10 AM
Hi
I have stm3210c-eval, I use stm32cubef11.zip as base. I imported LwIP_TCP_Echo_Client and ping works. I tried to implement uart capabilities on the LwIP_TCP_Echo_Client project. I first imported UART_TwoBoards_ComPolling and made it work with output display on hyperterminal. I then took the code as is and deleted the original files (main.c etc) from LwIP_TCP_Echo_Client project and put the src code from UART_TwoBoards_ComPolling. So actualy the same exact code runs on both projects. I run it and it got stack on HAL_UART_Transmit function without it actualy transmitting. What can be the cause of this? How would you sugest to solve this problem?Thanks,
Zohar