cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Value Line Discovery Board in Keil: ''Unknown Target Connected''

smithderek2000
Associate III
Posted on August 14, 2014 at 02:31

Hello,

   I'm testing the STM32F100 processor with STMicro L6474 motor driver for a new product. I'm testing with the STM32 Value Line Discovery board. I downloaded and installed Keil uVision, most recent release (5.11). I also downloaded and installed the legacy tools too.

   I downloaded the L6474 software example for the STM32 Value Line Discovery Board. I can open them in uVision, and build the example. But when I attempt to download to the board, I get an error ''Unknown Target Connected''.

In Options : Debug I selected ''ST-Link Debugger'' to use. And in Flash Download I selected STM32F10x Med-density Flash''.

I have verified that the USB device is showing up in Device Manager.

How do I get this to work? This is holding up development.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on August 14, 2014 at 03:58

The VL-Discovery probably should be ''ST-Link (Deprecated)'' if that's available as an option, as it's an ST-LINK V1 device.

Make sure you use SWD mode, and not JTAG, and make sure it is recognized in the dialog pane.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
smithderek2000
Associate III
Posted on August 14, 2014 at 23:36

There was no option for ''ST-Link (Deprecated)'' but switching to SWD mode worked and I am now able to download code to the device.

Thanks