STM32 F7 ADC specifications
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-12-08 2:36 PM
Posted on December 08, 2014 at 23:36
I would like if the F7 series will use the same ADC chip and if his maximum clock will still be 36 MHz .
If it is the case, the maximum possible ADC clock at 200 MHz will be 25 MHz?Thank you.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0