2015-08-21 12:04 AM
Hello All,
I started working/learning micripython using STM32F407 discovery board. The board I'm using is already with micropython (as my colleague used it earlier).I connected board to Windows PC and in ST Link utility I see this:12:24:40 : ST-LINK SN : 55FF7206507549544633208712:24:40 : ST-LINK Firmware version : V2J23S012:24:40 : Connected via SWD.12:24:40 : SWD Frequency = 1,8 MHz.12:24:40 : Connection mode : Normal.12:24:40 : Debug in Low Power mode enabled.and Colored LEDs are blinking, Now I want to run few micropython commands on board. I connected a different USB cable at CN5 and I don't see any COM port in device manager in windows. Need help.As of now I don't have a Linux PC to flash new binary on to the board, that's the reason I'm trying on Windows PCThanks #micropythonWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.