2011-03-08 12:38 PM
STM32 @ 16Mhz TXCO
2011-05-17 5:27 AM
Yes this will work, you need to review the clock trees in the reference manual.
The USBCLK = PLLCLK/1 or PLLCLK/1.5, permitting a 48 MHz or 72 MHz SYSCLK for USB operation. You could also technically run the CPU at 8 or 16 MHz, and have the PLL just run the USB. The AHB, APBx can be a fraction of the SYSCLK. The PLL can be driven by HSI/2, HSE, or HSE/2 An 6 or 12 MHz TCXO would also work.2011-05-17 5:27 AM
Thanks Clive,
I will write some more when I lunch the Project.