cancel
Showing results for 
Search instead for 
Did you mean: 

STm wifi module

elaroussi
Associate II
Posted on March 25, 2014 at 13:24

Hi,

Anyone of you have worked on WIFI? I need a small help related to that.

I need to develop an application that sends and receives some data via usart, cause I need to communicate with a wifi device (i'm using a stm32f4discovery board).

but the problem is that i can't find a wifi module which is compatible with my stm32f4

several questions running through my head

can i use any module found in the internet ?

 what about Software?

 what about compatibility?

also can i wired this module SG901-1098 from Sagrad directly to my stm32f4 board and making the necssary configuration to make it work (sending and receiving data in a standalone mode)?

the project idea is to make the system (STM32F4 discovrey Board and wifi module) operate in a standalone mode without the PC being used.

thx in advance 

S.Laaroussi
This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Posted on September 25, 2015 at 17:01

The ESP8266 seems to be quite prolific, and well priced.

Granted, I've only got 32 years of experience, so maybe it's me.

No, these things can get unmanageably complex. The code in the modules is usually a couple of orders of magnitude more complicated than the design they are being integrated into.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..