cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL PROTEUS-1 - Modal analysis using impact hammer

Ravide
Associate

Dear all, I'm trying to evaluate the IIS3DWB sensor using the STEVAL PROTEUS-1. Would it be possible to use the sensor to capture transient vibration e.g. Modal test using an impact hammer?

Is there an example script for STEVAL PROTEUS-1, to capture the data and save it to an SD card? The trigger signal will be manually activated prior to the impact and the data will be captured for 60 - 90 seconds. The sampling rate will be a min. of 20kHz as the highest frequency of interest is approx. 7kHz. Any advice would be much appreciated.

Thanks in advance,

best regards,

Ravi

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0