cancel
Showing results for 
Search instead for 
Did you mean: 

Stack misalignment

moretto
Associate
Posted on September 04, 2009 at 23:23

Stack misalignment

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
moretto
Associate
Posted on May 17, 2011 at 13:22

I use IAR toolchain and STM32F101C6T6 as target.

When I download my code to start debug the J-Link driver return the following error:

Stack pointer is setup to incorrect alignment. Stack addr=0xFFFFFFFF.

My application's main is empty. I just include the peripherals driver and IAR's startup file.

Can anyone help me?

Thanks.

Mauro.

picguy
Associate II
Posted on May 17, 2011 at 13:22

Did you setup the reset vector? On reset he word at 0000 goes to sp. The word at 0004 goes to pc. One might expect sp=FFFFFFFF if the reset vector is erased and not programmed.

16-32micros
Associate III
Posted on May 17, 2011 at 13:22

Hi Mauro,

You can try to run first the latest templates from our web site

http://www.st.com/stonline/products/support/micro/files/stm32f10x_stdperiph_lib.zip

then go to this subdirectory :

\stm32f10x_stdperiph_lib\Project\Template\EWARMv5

Do not forget to change ''your target'' as shown below since you use Low-density devices which is compatible with STM3210B-EVAL board, else you will get a similar error :-).

Hope this helps you.

Cheers,

STOne-32.

[ This message was edited by: STOne-32 on 05-09-2009 02:54 ]

jj
Associate II
Posted on May 17, 2011 at 13:22

Agree w/picguy.

However - more basic - have you tried your J-Link with an ''official'' eval/dev board? Always useful to have something ''known good'' to avoid the dreaded, ''maximum randomness.'' (i.e. new hw, new sw, new tool, new IDE etc)

ST-One32 advises that we check Segger site - download the newest sw for JLink.

I would beg/borrow/steal basic IAR or ST eval board - and get that to work before the debug of (I assume) your custom C6T6 pcb. Good luck...