cancel
Showing results for 
Search instead for 
Did you mean: 

st-vlink v2 no target connected

vivelavida911
Associate II
Posted on January 07, 2015 at 09:40

hi, im trying to connect a STM32F107VCT6 to flash it, but the st-linkv2 doesnt detect it.

I have conected pins:

4--GROUND

6--GROUND

7--SWDIO---------------------------PIN 72  MICROCONTROLER

8--GROUND

9--SECLK---------------------------PIN 76  MICROCONTROLER

10--GROUND

12-- GROUND.

14--GROUND

16--GROUND

18 --GROUND

20--GROUND

but still doesnt conect.

PLEASE HELP!!!

Its says that has no power supply detected and either doesnt detect the stm32 too.

#stm32f107vct6-no-detection
This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
Posted on January 08, 2015 at 00:21

the micro is autosupplied, so dont need 3.3 volts pin 1.

Whatever that means. The target voltage is put there by YOUR board to power the level converter buffers on the ST-LINK.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
vivelavida911
Associate II
Posted on January 08, 2015 at 21:56

ok, but... the maker of the pbc only have conected the pins 7, 9 and 12.

so ... may be damaged any component?... i have all the volts correct.

Posted on January 08, 2015 at 22:51

ok, but... the maker of the pcb only have connected the pins 7, 9 and 12.

 

so ... may be damaged any component?... i have all the volts correct.

And do either of these board designs work? Doesn't really sound like a component issue.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..