Skip to main content
morpeh89
Associate III
February 16, 2011
Question

ST Virtual COM example. What is the speed of data transfer via USB?

  • February 16, 2011
  • 11 replies
  • 2232 views
Posted on February 16, 2011 at 14:52

ST Virtual COM example. What is the speed of data transfer via USB?

    This topic has been closed for replies.

    11 replies

    tsuneo
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 14:25

    > Last year I attended a Microchip course that confirming these data.

    I advise to Microchip, to fire such a lazy instructor.

    He should check it by himself, before teaching it to others.

    Or, if he couldn't really get more than 640 Kbits/s (ie. 64 bytes/frame), he doesn't realize the relation of transfer-transactions. Not qualified for an instructor of USB course.

    > Do you have an example that I can use to make new test?

    Realize the relation of Transfer - Transactions, first.

    And then, you can write such a code by yourself immediately.

    It's the first hurdle for USB beginners (and the instructor should teach it).

    I've explained it on everywhere, for example,

    http://www.cygnal.org/ubb/Forum9/HTML/001627.html

    Tsuneo