cancel
Showing results for 
Search instead for 
Did you mean: 

ST link V2

izal muin
Associate
Posted on May 29, 2018 at 08:11

I need to program external memory using CLI. Conventional programming using the software is succesfull. Need to integrate the commands for the labview programming.

C:\Project\Programming\ST-LINK Utility>ST-LINK_CLI.exe -P assets.hex -EL MX25L512G_STM32F769I-DISCO.stldr

STM32 ST-LINK CLI v3.0.0.0

STM32 ST-LINK Command Line Interface

ST-LINK SN : 48FF6C067266535216230367

ST-LINK Firmware version : V2J29S7

Connected via SWD.

SWD Frequency = 4000K.

Target voltage = 3.1 V.

Connection mode : Normal.

Device ID:0x451

Device flash Size : 2048 Kbytes

Device family :STM32F76x

Loading file...

Flash Programming:

  File : assets.hex

  Address : 0x90000000

  External Loader File : MX25L512G_STM32F769I-DISCO.stldr

  Device Name          : MX25L512G_STM32F769I-DISCO

  Device Start Address : 0x90000000

  Device Size          : 0x04000000

  Device Type          : Nor Flash

Memory programming...

¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦ 0%

Timeout during flash programming

Error occured during erase operation!

Programming Complete.

is the  any additional parameter need to be type into it?  I have tried with the latest version seem not succesfullly done both using the GUI or CLI 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee
Posted on May 29, 2018 at 11:33

Hello

izal.muin

,

I recommend you to use the new

http://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-programmers/stm32cubeprog.html

software tool delivers device-programming and firmware upgrade for STM32 microcontrollers.

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen