cancel
Showing results for 
Search instead for 
Did you mean: 

ST-Link (SWD)// STM32F4Discovery

fhorvat
Associate
Posted on February 22, 2014 at 14:31

I used the discovery kit to prototype a control-board. The self developed board using the stm32F4 MPU works well. Thus far i flashed it with the st link debugger that is integrated into the kit, which worked fine. Now i've bought a st-link standalone debugger and tried to flash with it. Sadly the IDE throws the Error: ''Flash driver function execute error''. I upgraded the St-Link to the newest firmware, but that didn't help.

To verify that nothing wrong with my self-developed board i tried to flash the Discovery Board with the external ST-LINK (Jumper for internal ST-LINK pulled of, and the external ST-Link connected to these PINs; GND, and RST also connected), the error stayed the same ...

Is the St-Link i got broken, or am i doing somthing wrong?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Andrei Chichak
Lead II
Posted on February 25, 2014 at 00:10

You're doing something wrong. I just went through this. The onboard ST-Link module can either program the onboard processor or, by removing the jumpers, program an offboard processor.

If you want to use an external ST-Link to program your onboard processor, you have to pull SB3,5,7,9,11, and 12. This will isolate the onboard processor from the onboard ST-Link.

Then, you need to wire:

STLINK                            P1/P2

----------------------------------------

1 (VAPP)                           +3V

3 (GND)                            GND

7 (SWDIO)                        PA13

9 (SWCLK)                       PA14

15 (NRST)                         NRST

Pin 1 on the ST-Link is the pin on the 20 pin header closest to the designator CN3. As with all IDC 2x headers, the numbering is

1 2

3 4

5 6

7 8

and so on. In this case 1 is on the side with the notch, and the pins are beside each other 1,3,5,7,9,11,13,15,17, and 19.

I have used this setup for a few days now, along with Eclipse, OpenOCD, and GCC, to program my ST32F4Discovery board with the RTEMS RTOS. I think it may actually be faster than the onboard ST-Link, but I could be hallucinating.

frankmeyer9
Associate II
Posted on February 25, 2014 at 08:48

Is the St-Link i got broken, or am i doing somthing wrong?

 

I hope you realized that the standalone version of the st-link defaults to JTAG, not SWD.

Have you checked this in the settings of your flashing software ?

Since you connect only the SWD wires, you might need to change this to SWD.