cancel
Showing results for 
Search instead for 
Did you mean: 

ST application note AN3116: referenced examples cannot be found

juergen239955_stm1
Associate II
Posted on August 31, 2012 at 02:57

After reviewing the (very informative) application note on ''STM32's ADC modes

and their applications'', which is located at the site below, I was curious where I can find the numerous examples which are referenced in the note, and which allegedly are attached to it. Examples are:

- Dual_FastInterleaved, page 10

- Dual_AlternateTrigger, page 13

- Dual_Combined_Reg_Inj_Sumultaneous, page 14,  ... etc.

Thanks for your help,

JJ

http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/APPLICATION_NOTE/CD00258017.pdf

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Posted on August 31, 2012 at 03:23

A lot of the examples have percolated into the standard peripheral library example files.

Are you looking for the STM32F1xx parts or the more recent F2 or F4?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on August 31, 2012 at 05:24

After a bit of Googling I have this

http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/FIRMWARE/an3116.zip

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
juergen239955_stm1
Associate II
Posted on September 06, 2012 at 23:22

Muchos gracias! Exactly what I was looking for (exact version not so important, I just wanted to see the implementation as guidance).

Thanks again.

nanayakkaraan
Associate II
Posted on August 14, 2013 at 13:41

Hello,

At the moment I could not find sample Firmware in the given location, instead I came across those in the following location.

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/PF257864

May be ST have shifted the location.

Anyway thought it would be helpful to share this location, for the sake of someone else searching for the samples.

:)

Thanks.

-Anuradha.