2009-07-21 5:13 PM
SPI1 receive wrong data in normal mode but ok in debug
2011-05-17 4:18 AM
Hi, guys:
I am using STM32F103VBT6 with ULINK2 and KEIL uVision 3. I have STM32 SPI1 as slave, another MCU SPI as master, with CPOL and CPHA of slave and master all be set 0. Everything is ok when i use ULINK2 to debug, but after power reset, STM32 is in normal mode, STM32 always receive incorrect data. It seems that the receive data is half of correct data. However, if i set CPOL and CPHA of master all 0, and CPOL and CPHA of slave all 1, STM32 can reveive correct data in normal mode but incorrect in debug mode. Thank you very much for any advice...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.