Skip to main content
shafqathussnain
Associate
December 10, 2014
Question

SPI Slave is giving garbage values.

  • December 10, 2014
  • 3 replies
  • 938 views
Posted on December 10, 2014 at 19:15

I have configured my STM32F407 Discovery Board as slave with a STM8S00. The data sent by Master on MOSI is totally different from that which that my slave is receiving I have observed that data on the Digital Oscilloscope. Setting in the master is as follows: CPHA=1 CPOL=1 Master sends at Negative edge and samples at positive edge. SPI Clock is 4 MHz. It is also sending back different data that sent by a STM32F407 master.

Here is the code of main file:

#include ''stm32f4_discovery.h''

int i=0, IT_St=0;

int Rx_Buf[1000];

void SPI_TR(void);;

void n_Tick(int tk);

void n_Tick(int tk)

{

while(tk--)

{

}

}

void SPI_TR(void)

{

GPIO_InitTypeDef GPIO_SPI;

SPI_InitTypeDef My_SPI;

NVIC_InitTypeDef nvic;

EXTI_InitTypeDef itr;

RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);

//PA4=NSS  PA5=SCK  PA6=MISO  PA7=MOSI

GPIO_SPI.GPIO_Pin=GPIO_Pin_4 | GPIO_Pin_5 |  GPIO_Pin_6 | GPIO_Pin_7;

GPIO_SPI.GPIO_Mode=GPIO_Mode_AF;

GPIO_SPI.GPIO_PuPd=GPIO_PuPd_NOPULL;

GPIO_SPI.GPIO_OType=GPIO_OType_PP ;

GPIO_SPI.GPIO_Speed=GPIO_Speed_100MHz;

GPIO_Init(GPIOA, &GPIO_SPI);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_SPI1);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_SPI1);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_SPI1);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_SPI1);

  SPI_I2S_ITConfig(SPI1, SPI_I2S_IT_RXNE, ENABLE);

RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);

nvic.NVIC_IRQChannel=SPI1_IRQn;

nvic.NVIC_IRQChannelCmd = ENABLE;

nvic.NVIC_IRQChannelPreemptionPriority= 0;

  NVIC_Init(&nvic);

My_SPI.SPI_Direction = SPI_Direction_2Lines_FullDuplex;

My_SPI.SPI_Mode = SPI_Mode_Slave;

My_SPI.SPI_DataSize = SPI_DataSize_8b;

My_SPI.SPI_CPOL = SPI_CPOL_High;

My_SPI.SPI_CPHA = SPI_CPHA_2Edge;

My_SPI.SPI_NSS = SPI_NSS_Hard; // Configure it make high to low transition

//My_SPI.SPI_BaudRatePrescaler=SPI_BaudRatePrescaler_16;

My_SPI.SPI_FirstBit = SPI_FirstBit_MSB;

SPI_Init(SPI1, &My_SPI);

SPI_Cmd(SPI1, ENABLE);

}

void SPI1_IRQHandler()

{

Rx_Buf[i]=SPI_I2S_ReceiveData(SPI1);

  //i=SPI_I2S_ReceiveData(SPI1);

SPI_I2S_ClearFlag(SPI1, SPI_I2S_FLAG_RXNE);

SPI_I2S_ClearITPendingBit(SPI1, SPI_I2S_IT_RXNE);

SPI_I2S_SendData(SPI1, FIFO_STATUS_RX_FULL);

i++;

if(i>=1000)

i=0;

}

int main(void)

{

SPI_TR();

while(1)

{

}

  

}

    This topic has been closed for replies.

    3 replies

    waclawek.jan
    Super User
    December 10, 2014
    Posted on December 10, 2014 at 19:26

    Can you post examples of a stream transmitted by master, and corresponding data as the slave receives them?

    JW
    shafqathussnain
    Associate
    December 11, 2014
    Posted on December 11, 2014 at 06:34

    Actual Data Sent By Master: (MSB First) Observed on Digital Oscilloscope

    0000 0111 -> 1110 0000 (0xE0 Expected to be received)

    0101 0000 -> 0000 1010 (0x0A)

    0000 1000 -> 0001 0000 (0x10)

    1010 0101 -> 1010 0101 (0xA5)

    But Slave is providing following Data: (I don't know which Byte correspond to that sent by Master)

    0100 1011 (0x4B)

    0000 1111 (0xF)

    1010 0000 (0xA0)

    0001 0001 (0X11)

    waclawek.jan
    Super User
    December 11, 2014
    Posted on December 11, 2014 at 08:58

    > I don't know which Byte correspond to that sent by Master

    This makes your data worthless... Try to synchronize them somehow.

    Also, make sure you have consistent ground - always connect your oscilloscopes' ground to the receiver's ground.

    JW