2015-06-24 6:04 AM
To write multiple adress you sould use
Auto Address Increment (AAI) Word-Program Sequence This is the code. /************************************************************************/ /* PROCEDURE: EBSY */ /************************************************************************/ void EBSY() { sFLASH_CS_LOW(); /* enable device */ YYCM_SpiPut(0x70); /* send EBSY command */ sFLASH_CS_HIGH(); /* disable device */ } /************************************************************************/ /* PROCEDURE: DBSY */ /************************************************************************/ void DBSY() { sFLASH_CS_LOW(); /* enable device */ YYCM_SpiPut(0x80); /* send EBSY command */ sFLASH_CS_HIGH(); /* disable device */ } /************************************************************************/ /* PROCEDURE: WRDI */ /************************************************************************/ void WRDI() { sFLASH_CS_LOW(); /* enable device */ YYCM_SpiPut(0x04); /* send WRDI command */ sFLASH_CS_HIGH(); /* disable device */ } /************************************************************************/ /* PROCEDURE: Auto_Add_IncA */ //------Dikkat Sadece 2 nin katlari seklinde yazabiliyor AUTO increment // Auto Address Increment (AAI) Word-Program Sequence with Software End-of-Write Detection /************************************************************************/ void sFLASH_WritePage_AutoINC(uint8_t* pBuffer,unsigned long Dst,uint16_t NumByteToWrite) { //EBSY(); /* Enable SO as RY/BY# output if in AAI */ sFLASH_WriteEnable(); sFLASH_CS_LOW(); /* enable device */ YYCM_SpiPut(0xAD); /* send AAI command */ YYCM_SpiPut(((Dst & 0xFFFFFF) >> 16)); /* send 3 address bytes */ YYCM_SpiPut(((Dst & 0xFFFF) >> 8)); YYCM_SpiPut(Dst & 0xFF); YYCM_SpiPut(*pBuffer); /* send 1st byte to be programmed */ pBuffer++; YYCM_SpiPut(*pBuffer); /* send 2nd byte to be programmed */ pBuffer++; sFLASH_CS_HIGH(); /* disable device */ NumByteToWrite=NumByteToWrite-2; while (NumByteToWrite) //!!!Dikkat Bu Sekilde Calismiyor Otomatik Aderss artt1rma vs yok!!! { sFLASH_CS_LOW(); /* enable device */ YYCM_SpiPut(0xAD); /* send AAI command */ YYCM_SpiPut(*pBuffer); /* send 1st byte to be programmed */ pBuffer++; YYCM_SpiPut(*pBuffer); /* send 2nd byte to be programmed */ pBuffer++; sFLASH_CS_HIGH(); /* disable device */ NumByteToWrite=NumByteToWrite-2; } WRDI(); /* Exit AAI before executing DBSY */ //DBSY(); /* disable SO as RY/BY# output if in AAI */ sFLASH_WaitForWriteEnd(); }