2016-09-05 4:29 PM
I got the Discovery STM32F303VCT and i had to solder the SB10, because even if the UM1570-User Manual says the SB was made it wasn�t. I soldered to use printf with Keil.
After this board modification i got a lot of problems with interrupts; EXTI0_IRQn are redirected to EXTI9_5_IRQn and others like UART4 don�t work. Could these interruptions issues be related to made the SB10 ? regards, #sb #stm32f303vct #solder-bridge2016-09-05 7:04 PM
Connecting PB3 (SWO) to the ST-LINK doesn't strike me a causally related to the interrupt issues.
I wouldn't use printf() under interrupt, by that's a different matter.2016-09-08 9:37 AM