cancel
Showing results for 
Search instead for 
Did you mean: 

Should LSERDY assert with LSEBYP?

Uwe Bonnes
Chief

Hello,

should LSERDY assert with LSEBYP?

I have a SIT1533 (32.768 khz Mems ocsillator) connected to PC14/OSC32IN on a L412. I first reset the backup domain, than I enable LSEBYP and with next command I enable LSEON. On a cold start, where the SIT1533 may need 500 ms, LSERDY never asserts, also OSCIN is toggling when I check with a scope.

Otherwise why does the sequence

  • reset BCDR
  • wait that LSERDY is de-asserted
  • set LSEBYP
  • wait untill LSEBY is asserted
  • set LSEON
  • wait until LSEON is asserted
  • apply clk to OSC32 in

not set LSERDY?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Hello.

LSERDY indicates crystal's oscillation stability.

I didn't found any mentioned relationship between these two bits, but also is not mentioned the state of LSERDY in case of using external osc. (probably undefined)