cancel
Showing results for 
Search instead for 
Did you mean: 

SDIO can't read more than 511 blocks

unparagoned
Associate II
Posted on June 26, 2012 at 22:41

I'm using the standard STM libaries. I'm using SDIO with DMA. It works perfectly when reading up to 511 blocks but as soon as I try and read 512 blocks it stops working. It would successfully transfer 511 blocks then stop and become non-responsive. It seems like I must be missing something obvious due to the number of blocks it stops on. I looked at the varaibles used and registers but 512 blocks of 512 bytes doesn't seem like it would overun any of them.

I guess the relevant code is below. Where if

NumberOfBlocks

is above 511 it stops working.

 SDIO_DataInitStructure.

SDIO_DataTimeOut

= SD_DATATIMEOUT;

SDIO_DataInitStructure.

SDIO_DataLength

= NumberOfBlocks * BlockSize;

SDIO_DataInitStructure.

SDIO_DataBlockSize

= (

uint32_t

) 9 << 4;

SDIO_DataInitStructure.

SDIO_TransferDir

= SDIO_TransferDir_ToSDIO;

SDIO_DataInitStructure.

SDIO_TransferMode

= SDIO_TransferMode_Block ;

SDIO_DataInitStructure.

SDIO_DPSM

= SDIO_DPSM_Enable;

SDIO_DataConfig

(&SDIO_DataInitStructure);

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on June 26, 2012 at 23:01

Not really rocket science here, but a quick back of the envelope yields

512 x 512 = 262144 (256KB)

DMA length count 16-bit units, max data transfer width 32-bits

65535 * 4 = 262140

The cards might well throw in additional limits.

You might be able to handle more by chaining DMA transfers at TC.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
unparagoned
Associate II
Posted on June 27, 2012 at 20:33

Thanks clive1 I knew it would be fairly obvious once I knew where to look but was looking in the wrong place. I was looking at the SDIO limits rather than DMA. Thanks.

Posted on June 27, 2012 at 21:51

Personally I think having 16-bit counters and timers on a 32-bit micro is a bit of a cop-out.

I suppose having ridiculously large DMA transfers could be problematic, the limit should at least be able to act on the entire external memory buffer space.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..