cancel
Showing results for 
Search instead for 
Did you mean: 

SD and FATFS on STM32F7xx issue with card init, how to change the source files for CubeMX

Stefan M�ller
Associate II
Posted on October 30, 2017 at 12:46

Hi to everyone,

I just bought STM32F769 Disco Board as platform to develop SW for my next project. I'm using CubeMX 4.23, F7xx FW package 1.8.0 and latest SW4STM32. For the CubeMX I was choosing the processor type and not the Disco Board as later on it will be an own PCB and I wanted to be as much independent as possible.

As I tried to get SD Card and FAT FS running I realized that Disk Init and therefore Hardware init on the MCU seems to go wrong. I debugged it down and found 2 issues in the code generated by CubeMX:

First is very simple as the card detect pin needs to be inversed in the fatfs_platform.c file to fit the Disco Board.

Second issue is that the SD_initialize function of sd_diskio.c just does nothing (ok it calls CheckStatus but doesn't init anything)

Therefore I modified from original code:

/**

* @brief Initializes a Drive

* @

param

lun

: not used

* @

retval

DSTATUS: Operation status

*/

DSTATUS

SD_initialize(

BYTE

lun)

{

return

SD_CheckStatus(lun);

}

to:

/**

  * @brief  Initializes a Drive

  * @param  lun : not used

  * @retval DSTATUS: Operation status

  */

DSTATUS SD_initialize(BYTE lun)

{

 Stat = STA_NOINIT;

 if(BSP_SD_Init() == MSD_OK)

 {

  return SD_CheckStatus(lun);

 }

 return Stat;

}

So far it works all fine...

Now my questions:

1: Was this the right way to solve it or did I oversee something?

2: How/where can I Change the source files for the CubeMX so that after newly generating the Project files my changes are kept? I was looking for the .c files in the FW package but there are everywhere in  the examples but nowhere seems to be a source Location for the cubeMX....

Thanks in advance

Stefan

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Imen.D
ST Employee
Posted on October 31, 2017 at 08:34

Hello

s.mueller

,

Thank you for your contribution. Your issue is raised internally to the appropriate teamfor further review.

We will come back to you as soon as possible.

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
FCR
ST Employee
Posted on November 23, 2017 at 11:49

Hello

s.mueller

,

The issue will be solved in the next official release (4.24).

Our apologies again for that regression impacting the series supporting FatFS R0.12c (F4, F7, H7 and L4).

Back to your questions, in fact, modifying generated code is useless unless code is added in what we call 'user sections'.

You will find different places in some files (such as sd_diskio.c) looking like:

/* USER CODE BEGIN sectionName */

/* place for user code */

/* USER CODE END sectionName */

The user code added there will be kept when generating again the project.

As a workaround, in order to fix the current issue before the 4.24 is available, I can suggest you a patch, using the existing user sections:

/* USER CODE BEGIN beforeFunctionSection */

/* can be used to modify / undefine following code or add new code */

#ifdef BROKEN_CODE /* Note: not defined, then following code will be ignored when preprocessing the C file */

/* USER CODE END beforeFunctionSection */

/* Private functions ---------------------------------------------------------*/

static DSTATUS SD_CheckStatus(BYTE lun)

{

Stat = STA_NOINIT;

if(BSP_SD_GetCardState() == MSD_OK)

{

Stat &= ~STA_NOINIT;

}

return Stat;

}

/**

* @brief Initializes a Drive

* @param lun : not used

* @retval DSTATUS: Operation status

*/

DSTATUS SD_initialize(BYTE lun)

{

return SD_CheckStatus(lun);

}

/**

* @brief Gets Disk Status

* @param lun : not used

* @retval DSTATUS: Operation status

*/

DSTATUS SD_status(BYTE lun)

{

return SD_CheckStatus(lun);

}

/* USER CODE BEGIN beforeReadSection */

#else

static DSTATUS SD_CheckStatus(BYTE lun)

{

Stat = STA_NOINIT;

if(BSP_SD_GetCardState() == MSD_OK)

{

Stat &= ~STA_NOINIT;

}

return Stat;

}

/**

* @brief Initializes a Drive

* @param lun : not used

* @retval DSTATUS: Operation status

*/

DSTATUS SD_initialize(BYTE lun)

{

Stat = STA_NOINIT;

if(BSP_SD_Init() == MSD_OK)

{

return SD_CheckStatus(lun);

}

return Stat;

}

/**

* @brief Gets Disk Status

* @param lun : not used

* @retval DSTATUS: Operation status

*/

DSTATUS SD_status(BYTE lun)

{

return SD_CheckStatus(lun);

}

#endif

/* USER CODE END beforeReadSection */

Not that beautiful, I agree, but should fix the issue (till the 4.2.4.0 solves it in a cleaner way).

Let us know if it does not.

Regards,

Fred

Stefan1
Associate III
Posted on January 05, 2018 at 11:53

Hi Fred,

Do you also have a fix for fatfs in combination with FreeRTOS?

So far i found that the CubeMX generated code is also missing the code to create the SD_Queue. (I found it in another example)

        /* Create SD operation Queue */

        osMessageQDef(SD_Queue, QUEUE_SIZE, uint16_t);

        SDQueueID = osMessageCreate (osMessageQ(SD_Queue), NULL);

That got me further with the debugging, but it is still not working so I am still missing something.

Board: STM32F769I-EVAL

Regards

Stefan

Posted on January 10, 2018 at 15:03

Hi Stefan,

watch out here:

https://community.st.com/0D50X00009bMM8bSAG

Best regards

Stefan