cancel
Showing results for 
Search instead for 
Did you mean: 

Sample Capture Only on External Trigger

JRick.1
Associate

Hi:

Is is possible to configure the LSM6DSOX to only capture data (Accel and Gyro) when an external trigger is given? This would be an interrupt from a host processor. The trigger may or may not be a fixed consistent frequency. I am aware of the DEN triggering where the closest sample to the external trigger is captured - can the sample be captured only when the external signal happens?

Thanks,

Joe

Follow up: Perhaps a better way to ask this: Is there a different ST Micro IMU that can be triggered to read acceleration/gyro conditions using an external signal? The LSM6DSOX does not seem to be externally triggerable.

Thanks,

Joe

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0