cancel
Showing results for 
Search instead for 
Did you mean: 

RTC design recommendation

gsantha
Associate II
Posted on November 27, 2011 at 19:53

Hi!

In my recent design I'd like track the time/date using the RTC peripherial of the STM32L152. If I'm not wrong, the RTC is only active when the MCUs power supply is on. I want the clock to run during powered down periods. How can I do that? Well before I was using external RTC chips equipped with backup battery VBAT power pins - has the STM32L152 VBAT pin or any similar?

Thanks, Greg73
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on November 28, 2011 at 20:06

The presumption is that the STM32L152 is running off a battery. Put it in STANDBY, it will turn off VCore and it should draw a few uAmp with the RTC ticking off LSI.

You'd put a battery and charger circuit upstream from the device.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
gsantha
Associate II
Posted on November 30, 2011 at 15:04

Thank you clive1. It is certainly a decent approach however I don't really like the idea to implement a battery charger subcircuit. I'm experimenting with diode ORing right now.