RTC and reset problem
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-03-31 5:20 AM
Posted on March 31, 2016 at 14:20
Hi to all,
I encounterd a problem using Real Time Clock. After I initilaized it, everything seems to work, but when I reset MCU it stops and I can restart my board only powering it off and then on again. Hereafter there is my code: CLOCK INITIALIZATION ========================================================== void SystemInit() { /*-------------------------------- HSE Configuration -----------------------*/ if(RCC->CR & RCC_CR_HSEBYP) RCC->CR &= ~RCC_CR_HSEBYP; // if HSE bypass, disable it if(!(RCC->CR & RCC_CR_HSEON)) // Check if HSE is on { RCC->CR |= RCC_CR_HSEON; // if not, just enable it while((RCC->CR & RCC_CR_HSERDY) == 0); // Wait for HSE being ready } /*-------------------------------- PLL Configuration -----------------------*/ if(RCC->CR & RCC_CR_PLLON) RCC->CR &= ~RCC_CR_PLLON; //Disable PLL while(RCC->CR & RCC_CR_PLLRDY); // Wait for PLL disabled RCC->CFGR |= 4<<18 | 1<<16; //PLLMUL6<<18 | PLLSRC<<16 (HSE) RCC->CFGR2 = 0x0000; //RCC_CFGR2_PREDIV_DIV1; // RCC->CR |= 0x01<<24; //PLLON while(!(RCC->CR & RCC_CR_PLLRDY)); // Wait for PLL enabled if(!(RCC->CFGR & RCC_CFGR_SWS_PLL)) RCC->CFGR &= 0xFFFFFFFC; // if PLL is not SystemClock, set PLL as SystemClock RCC->CFGR |= RCC_CFGR_SW_PLL; RCC->CFGR &= ~(RCC_CFGR_HPRE | RCC_CFGR_PPRE); //AHB and APB not divided /*-------------------------------- LSI Configuration -----------------------*/ if(!(RCC->CSR & RCC_CSR_LSION)) RCC->CSR |= RCC_CSR_LSION; //Enable LSI while(!(RCC->CSR & RCC_CSR_LSIRDY)); // Wait for LSI ready RCC->CIR = 0x00000000; // Disable all interrupts return; } ========================================================== RTC INITIALIZATION ========================================================== MYRTC::MYRTC() { uint8_t i; uint32_t t; if((RCC->BDCR & RCC_BDCR_RTCSEL) != (RCC_BDCR_RTCSEL_LSI & RCC_BDCR_RTCSEL)) // If RTC Clock is not LSI, just change it to LSI { RCC->APB1ENR |= RCC_APB1ENR_PWREN; // Enable power clock PWR->CR |= PWR_CR_DBP; // Enable write access to Backup domain i=0; while(((PWR->CR & PWR_CR_DBP) == 0) && (i++<10)) Delay(1); // Wait for write access enabled t = (RCC->BDCR & ~(RCC_BDCR_RTCSEL)); // Save BDCR value RCC->BDCR |= RCC_BDCR_BDRST; // Reset RCC->BDCR &= ~RCC_BDCR_BDRST; // End reset RCC->BDCR = t; // Restore register RCC->BDCR |= RCC_BDCR_RTCSEL_LSI; // Set LSI as RTC clock } if(!(RCC->BDCR & RCC_BDCR_RTCEN)) RCC->BDCR |= RCC_BDCR_RTCEN; // Enable RTC clock RTC->WPR = 0xCA; RTC->WPR = 0x53; // Enable register writing RTC->ISR |= RTC_ISR_INIT; // Enable init phase i=0; while(((RTC->ISR & RTC_ISR_INITF) != RTC_ISR_INITF) && (i++<10000)); // Wait for system ready RTC->PRER = 0x007F0137; // Set prescaler for 1Hz from 40KHz (LSI) RTC->ISR &=~ RTC_ISR_INIT; // Disable init phase RTC->WPR = 0xFE; RTC->WPR = 0x64; // Disable write access for RTC registers PWR->CR &= ~PWR_CR_DBP; // Disable write access to Backup domain } ========================================================== I followed what I found in the user manual and in CubeMX code, so I do not understand why a reset crashes everything. Do I forgot something? Thank you Freya
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-03-31 6:10 AM
Posted on March 31, 2016 at 15:10
Hi Freya,
It seems that your problem is coming from a bad switching between Power-ON and resuming from Standby/RESET states like this [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32F437%20exiting%20standby%20incorrectly¤tviews=63]request.
Take a look to my recommendation there. -Hannibal-Hi to all,
I encounterd a problem using Real Time Clock. After I initilaized it, everything seems to work, but when I reset MCU it stops and I can restart my board only powering it off and then on again. Hereafter there is my code: CLOCK INITIALIZATION ========================================================== void SystemInit() { /*-------------------------------- HSE Configuration -----------------------*/ if(RCC->CR & RCC_CR_HSEBYP) RCC->CR &= ~RCC_CR_HSEBYP; // if HSE bypass, disable it if(!(RCC->CR & RCC_CR_HSEON)) // Check if HSE is on { RCC->CR |= RCC_CR_HSEON; // if not, just enable it while((RCC->CR & RCC_CR_HSERDY) == 0); // Wait for HSE being ready } /*-------------------------------- PLL Configuration -----------------------*/ if(RCC->CR & RCC_CR_PLLON) RCC->CR &= ~RCC_CR_PLLON; //Disable PLL while(RCC->CR & RCC_CR_PLLRDY); // Wait for PLL disabled RCC->CFGR |= 4<<18 | 1<<16; //PLLMUL6<<18 | PLLSRC<<16 (HSE) RCC->CFGR2 = 0x0000; //RCC_CFGR2_PREDIV_DIV1; // RCC->CR |= 0x01<<24; //PLLON while(!(RCC->CR & RCC_CR_PLLRDY)); // Wait for PLL enabled if(!(RCC->CFGR & RCC_CFGR_SWS_PLL)) RCC->CFGR &= 0xFFFFFFFC; // if PLL is not SystemClock, set PLL as SystemClock RCC->CFGR |= RCC_CFGR_SW_PLL; RCC->CFGR &= ~(RCC_CFGR_HPRE | RCC_CFGR_PPRE); //AHB and APB not divided /*-------------------------------- LSI Configuration -----------------------*/ if(!(RCC->CSR & RCC_CSR_LSION)) RCC->CSR |= RCC_CSR_LSION; //Enable LSI while(!(RCC->CSR & RCC_CSR_LSIRDY)); // Wait for LSI ready RCC->CIR = 0x00000000; // Disable all interrupts return; } ========================================================== RTC INITIALIZATION ========================================================== MYRTC::MYRTC() { uint8_t i; uint32_t t; if((RCC->BDCR & RCC_BDCR_RTCSEL) != (RCC_BDCR_RTCSEL_LSI & RCC_BDCR_RTCSEL)) // If RTC Clock is not LSI, just change it to LSI { RCC->APB1ENR |= RCC_APB1ENR_PWREN; // Enable power clock PWR->CR |= PWR_CR_DBP; // Enable write access to Backup domain i=0; while(((PWR->CR & PWR_CR_DBP) == 0) && (i++<10)) Delay(1); // Wait for write access enabled t = (RCC->BDCR & ~(RCC_BDCR_RTCSEL)); // Save BDCR value RCC->BDCR |= RCC_BDCR_BDRST; // Reset RCC->BDCR &= ~RCC_BDCR_BDRST; // End reset RCC->BDCR = t; // Restore register RCC->BDCR |= RCC_BDCR_RTCSEL_LSI; // Set LSI as RTC clock } if(!(RCC->BDCR & RCC_BDCR_RTCEN)) RCC->BDCR |= RCC_BDCR_RTCEN; // Enable RTC clock RTC->WPR = 0xCA; RTC->WPR = 0x53; // Enable register writing RTC->ISR |= RTC_ISR_INIT; // Enable init phase i=0; while(((RTC->ISR & RTC_ISR_INITF) != RTC_ISR_INITF) && (i++<10000)); // Wait for system ready RTC->PRER = 0x007F0137; // Set prescaler for 1Hz from 40KHz (LSI) RTC->ISR &=~ RTC_ISR_INIT; // Disable init phase RTC->WPR = 0xFE; RTC->WPR = 0x64; // Disable write access for RTC registers PWR->CR &= ~PWR_CR_DBP; // Disable write access to Backup domain } ========================================================== I followed what I found in the user manual and in CubeMX code, so I do not understand why a reset crashes everything. Do I forgot something? Thank you FreyaOptions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-04-01 8:25 AM
Posted on April 01, 2016 at 17:25
Hi Hannibal,
indeed I do not want to put mcu in stanby or any other state. In my project mcu is on and stay on. I followed what I found to configure RTC. Now I changed sligthy initialization routine and reset is wworking properly, but I encounterd another problem, that is TR register is updated discontinuously. In other worlds, I read RTC_TR register more or less every second an I get the same values for several times and than the new value for some rondom times. For example: 7 for 10 times then 17 and it remains 17 for 20 times then 37 and so on. Now I try to check registers as suggested in your hint, but I do not understand what's wrong. Freya