cancel
Showing results for 
Search instead for 
Did you mean: 

Reseting the STLM75 Temperature sensor

daneichenwald1
Associate
Posted on April 17, 2009 at 15:23

Reseting the STLM75 Temperature sensor

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
daneichenwald1
Associate
Posted on May 17, 2011 at 13:10

I have my I2C drivers working as I can read and write to I2C devices. I'm working with the STLM75 Temperature sensor on the eval board. However, I noticed that if an I2C transfer gets interrupted, I can no longer talk to that device. The simplest case is:

1. Generate a START

2. Reset the processor

3. Generate a START

4. Write Addr -> Always generates Acknowledge Failure Error

5. Reset the processor

6. Works fine

I've tried generating various combinations of START/STOPs on every reset, but I can't seem to reset the temp sensor. (if that is even the problem) My code is basically taken directly from STM eval example.

Thanks in advance!

Dan

nanayakkaraan
Associate II
Posted on May 17, 2011 at 13:10

Hello Dan,

I am also facing the same problem you did, in I2C communication with STLM75 temperature sensor.

''Write Addr -> Always generates Acknowledge Failure Error ''

I have been receiving this error and trying to figure out how to overcome it.

Have you found any solutions?

Any advice on this matter is appreciated.

Thank you.