cancel
Showing results for 
Search instead for 
Did you mean: 

Reset

psandesh007
Associate II
Posted on August 01, 2013 at 15:34

Im doing reset in the STM32F103RBT6 board ...

Im updating the data in seven segment display and when i pressed reset switch which was connected to hardware reset , it was hanging up the present data in display and not cleared.

Is there any handler for the reset to clear all and bring back to original state when i pressed the reset switch.

#poorly-framed-question
This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
Posted on August 01, 2013 at 16:47

We know nothing about your board, or how the display is configured.

If the display latches data, then you'll need to attach the SAME async reset as you're supplying the processor. Failing that you'll need to add your own code to manually reset/reconfigure the display.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
psandesh007
Associate II
Posted on August 02, 2013 at 10:46

ok sorry.

Posted on August 02, 2013 at 13:12

Don't be sorry.

I was trying to get a better idea of what exactly you had connected, and how you programmed it currently. It's very hard to remotely trouble-shoot problems when the interface isn't clearly defined.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
psandesh007
Associate II
Posted on August 12, 2013 at 12:55

What Actually i wanted is , Interrupt handler (IRQ_Handler)  for Reset (NRST -> Pin No 7)  in the Board No STM32F103RBT6. 

Posted on August 12, 2013 at 19:39

Like Reset_Handler?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
psandesh007
Associate II
Posted on August 13, 2013 at 09:46

Yes, right (Reset_Handler).. 

Im trying different methods to find that Reset_Handler, but still not getting .  
crt2
Associate II
Posted on August 13, 2013 at 10:55

I dont know what lib you're using but in STDPeriph is: stm32f10x_vector.c where you can find Reset_Handler in .isr_vectors function.

psandesh007
Associate II
Posted on August 17, 2013 at 12:27

Ok surely i will try , if i got solution i will update clearly .. 

Thank You all .