cancel
Showing results for 
Search instead for 
Did you mean: 

Reading Device id using STM32 Flash Loader Demonstrator command line

Will Justin
Associate II
Posted on June 22, 2017 at 17:02

Just wanted to use the Flash Loader command Line to check Device id/Signature. I am sure whether that is possible.  I have attached a picture of the STM Command Line

Thanks

WJ

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on June 22, 2017 at 19:42

The addresses of the DBGMCU DEV ID and the Unique ID are in the Reference Manuals for the specific STM32 part in question

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on June 22, 2017 at 22:05

Hi Clive,

Here is picture of the STMFlash Loader.exe that I am using to communicate with STM32F100 chip. As you could see I do not see any command for DEVICE id or Device signature. Maybe I am using the wrong user software. Flash Loader v2.6

________________

Attachments :

image.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyXQ&d=%2Fa%2F0X0000000b9s%2Fq64.NOj0B41gOmiwU_wLJeh1z87EhYsaRYnucRepTN8&asPdf=false
Posted on June 23, 2017 at 10:22

Hi

justin1269

,

Try to use the latest version of flash loader v2.8.0

Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen